6/13/2013 2:37 PM | |
Joined: 4/24/2006 Last visit: 9/24/2024 Posts: 8742 Rating: (1168)
|
Hello malbec, Please have a look at the following link: Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? But very important: The version of Configuration software (WinCC flexible 2008 SP3) must be the same as the Runtime software. So please use alse WinCC flexible 2008 SP3 RT on panel PC. Best regards, Wizard |
6/13/2013 3:31 PM | |
Posts: 54 Rating: (0) |
Is it possible to upgrade the panel from SP2 to SP3? |
6/19/2013 1:05 PM | |
Posts: 3037 Rating: (192)
|
Hello, How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet? Tweety |
6/20/2013 11:27 AM | |
Posts: 54 Rating: (0) |
Communication problem solved. Still have a problem that it does not start automaticlly
|
6/20/2013 11:40 AM | |
Joined: 4/24/2006 Last visit: 9/24/2024 Posts: 8742 Rating: (1168)
|
Hello malbec, Have you seen this link: http://support.automation.siemens.com/WW/view/en/32813726 Best regards, Wizard |
6/20/2013 12:56 PM | |
Posts: 54 Rating: (0) |
OK, thanks. Now the only problem left if the transfer. I guess that as long as I have SP2 on the panel and SP3 on my PC it won't work. right?
|
Follow us on