Industry Online Support
Technical Forum
8/24/2010 11:16 PM | |
Posts: 2 Rating: (0) |
Anybody out there lend a hand, I have a few analogue inputs that I need to display on a TP177. When monitoring themin Step 7 I can see them all fine. If I put them individually onto the TP177 then once again they are okay, but as soon as I put more than one on, then only the last one reads. Attached is my program, I suspect the fault lies there, Would be grateful if someone could point me in the right direction. Thanks Len. AttachmentTechnip240810.zip (57 Downloads) |