5/18/2009 1:41 PM | |
Joined: 4/24/2008 Last visit: 8/2/2024 Posts: 213 Rating: (16) |
I see no error in the picture. 0V =0; 10V= 27648 0V =0; 10V=120 0=0; 120=27648 7376 = 32 = 2,67V the FC works like you have parametrise it. Maybe this FAQ http://support.automation.siemens.com/WW/view/en/1765297will help you to understand the function. |
|
|
5/18/2009 10:14 PM | |
Posts: 10 Rating: (0) |
Sorry for the spam, but I'd like to attach my scale FC too. The inputs to the FC are real values (Min_in = 0, max_in=27648, Min_out = 0, Max_out =120, analoginput = PIW752 and output is MD0 (Analog_input)) I don't see how this could affect setting and resetting of memorybits. Thanks for any input :) AttachmentFC3.pdf (325 Downloads) |
Follow us on