5/11/2021 1:02 AM | |
Joined: 9/9/2019 Last visit: 11/2/2023 Posts: 18 Rating: (0) |
Hi Experts... I'm having some troubles trying to download the configuration from a PCS7 ES/OS (SIMATIC RACK PC) to an OS (SIMATIC BOX PC) I can ping between them over TerminalBUS an also do a remote desktop sesion between them so that means that the network is ok and working (I think) I've already deactivate all the firewall protections Nevetheless I got this error while trying to download the configuration from the netpro, and also from the HW config I already import the .xdb file to configure the station (trough a windows network shared folder [The station configurator editor is online mode already]) What else can I do ? Thanks you a lot, nice day ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/11/2021 10:40:36New subject after splitting |
|
5/12/2021 7:16 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi Infinit5000, I guess that you configure the wrong network adapter in SIMATIC Shell (for more information see the FAQ How do you use the SIMATIC shell to configure the terminal bus of a WinCC station?). With regards |
This contribution was helpful to1 thankful Users |
5/12/2021 11:43 AM | |
Joined: 3/14/2008 Last visit: 9/23/2024 Posts: 2096 Rating: (938)
|
If you have configured via PLC->Configure, then download the NetPro configuration of the station so the whole configuration is known to the PC station. Then execute PLC>Download |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on