7/3/2007 7:38 PM | |
Joined: 1/22/2006 Last visit: 10/8/2020 Posts: 73 Rating: (0) |
Dear Everyone, Today I have faced a problem regarding channel 0 of the 331-7KB02-0AB0 AI 2X12 bit module. I have attached the wiring diagram. step 1. I have used digital meter to measure 4-20mA current by removing wire at terminal no.2 (of module) by keeping the meter in series with terminal no.2 ----- Found No current. step 2. I removed wire at terminal no.2 (kept it open) and connected the meter in series with terminal no.3 (of module).....I have found current in accordance with pressure. Does it mean that channel0 is faulty? There are no other faulty indications as well as hardware diagnostics is also ok. Thanks in advance. Attachment331_7KB02_0AB0.zip (250 Downloads) |
7/4/2007 6:05 AM | |
Posts: 54 Rating: (0) |
what is the position of ur connector 2 wire current or 4 wire current in the back of the module |
7/6/2007 2:14 PM | |
Joined: 1/22/2006 Last visit: 10/8/2020 Posts: 73 Rating: (0) |
Can you please tell me what should I do with terminals 10 and 11 for this 2DMU connection. Do I need to connect them to ground or left them not wired?? AttachmentSM331_7KB02_0AB0.pdf (259 Downloads) |
7/7/2007 5:40 AM | |
Posts: 15 Rating: (0) |
hi all |
Follow us on