4/30/2018 3:52 PM | |
Posts: 1 Rating: (0) |
Hi, I am trying to use TST (Tia selection Tool) and export the hardware configuration In Eplan and Tia V15. Unfortunately, things are not running as smoothly as wished. To start with I did a small project in TST using components that we use often, I did 2 exports, one for Tia and one for ECAD. To import to Eplan I had to change some fields in the article databank, but after this was done it was possible to import the hardware configuration to Eplan. The only thing that I couldn't import was the ET200ISP, IM152-1 INTERFACE MODULE, the base units for the ET200SP where imported without problems ( tst_to_eplan.jpg)(tst_to_eplan.aml) Then I imported the file created in TST (Tia export) in Tia V15. Again I imported without errors but the information for base units for the ET200Sp was lost (es200sp.jpg and et200sp_tia.jpg) after opening the AML file ( tst_to_tia.aml) I could see that no information regarding the base units was there. I changed in tia the base units so that the project was the same as the initial project in TST and did an export (tia_to_eplan_baseunitchanged.aml). This File was imported in Eplan and now I had the ET200ISP, IM152-1 INTERFACE MODULE (from_tia_in_plan.Jpeg +70A2) but the information regarding the ET200SP base units was missing again. I did a graphic and I uploaded the files and pictures, I hope this will help to better understand my workflow. We can see the advantage of TST, because that way we always use the newest components, ideally I would like to use the export and import functions in Tia and Eplan, but it looks like I am missing something. Has anyone come across similar problems? Thank you Tojeira Attachmentforum.zip (78 Downloads) |
8/30/2018 9:43 AM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Yes, we are facing same problems TST 2018 AML ECAD exported file not working in ePLAN V2.7 Applying these steps but not successful. EPLAN Electric P8, Version 2.7: Siemens TIA Portal Interface |
Last edited by: Jen_Moderator at: 8/30/2018 1:09:08 PMInserted video. MS |
|
Follow us on