7/2/2015 7:57 AM | |
Joined: 5/20/2015 Last visit: 4/24/2024 Posts: 216 Rating: (3) |
dear all, have a great day, gabbar is back with new query, and hope my masters will guide me as usual, and it is, what exactly mean by 2dp, if regards with cpu 315 2dp, is it possible to configur two no. of different master dp bus and run both at same time with different dp devices each master bus, actually i had seen that we can configure many dp master but at time in hardware structure i am getting only one.
please help ASAP.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/2/2015 10:03:52 AMNew subject after splitting Let's do it... |
|
7/3/2015 9:23 AM | |
Joined: 5/20/2015 Last visit: 4/24/2024 Posts: 216 Rating: (3) |
THIS IMAGE WILL MAKE YOU EASY... PLEASE GO THRUGH, THAT IS WHAT I HOPING FOR... |
Let's do it... |
|
7/3/2015 11:23 AM | |
Posts: 1058 Rating: (93) |
Hello gabbar, you do not describe precisely, but I assume you have this CPU: CPU 315-2 DP 6ES7315-2AH14-0AB0 As you can see in Manual CPU 31xC and CPU 31x: Technical specifications this CPU has 2 interfaces. Interface X1 is MPI only (no DP master or DP slave functionality) and interface X2 is either DP master or DP slave. To do a HW-configuration like you want you would need a different CPU: CPU 315T-2 DP 6ES7 315-6TH13-0AB0 There is only one character more(T) in name, but as you can see in manual CPU 31xT: Technical data there are also 2 interfaces, but with different functionality. Interface X1 can be either MPI, DP master or DP slave - and interface X3 is DP master only. So with the CPU 315T-2 DP you can do the HW configuration you want, but not with CPU 315-2 DP. regards |
Follow us on