3/25/2009 12:24 PM | |
Joined: 4/10/2006 Last visit: 9/19/2024 Posts: 930 Rating: (2) |
Ok Wizard but i must create an "stack register" where appear the last change parameters... I thought to use the storical alarms and the alarm call that I need...BUT isn't alarm!! In the line i insert the old variable and the new variable...(see Attachment) every time someone changes a setting machine, log in this way changed what was displaying it as an archive... but if they see two, it is wrong .....
sure that we can not do anything? Thank you roby Attachmentmessage.pdf (79 Downloads) |
Setting of my PG M6 Siemens |
|
3/25/2009 2:13 PM | |
Joined: 4/10/2006 Last visit: 9/19/2024 Posts: 930 Rating: (2) |
Ok. Everything is all right and work correctly. When the alarm's bit is high the warning is shown with an incoming event. When the alarm's bit islow the warning is shown with anoutgoing event. I just want the warning of incoming event but not both. Now is clear? Thank you, Roby I use the panel OP177B. I attach a document that I hope help you to understand what I really want. Please help me because I will send the machine tomorrow. Attachmentmessage1.pdf (104 Downloads) |
Last edited by: Roby at: 3/25/2009 2:38 PMLast edited by: Roby at: 3/25/2009 2:23 PMSetting of my PG M6 Siemens |
|
3/26/2009 9:46 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi I meant the same like wizard. The main thing is that it works. Bye |
Follow us on