7/8/2021 8:39 AM | |
Joined: 5/21/2021 Last visit: 7/5/2024 Posts: 11 Rating: (0) |
UPDATE: I have now solved the problem. Unfortunately, I cannot say exactly what caused it, as I did several things at once before uploading the app to the Industrial Edge again. 1.) The first thing I did was update Docker to the latest version, which had been available for a few days 2.) then I increased the memory limit in the Docker-compose to 500 MB 3.) and lastly I assigned a new tag (testapp:dev -> testapp:1.0.5) and then executed the command "docker-compose build" again After following these three steps, I uploaded the app again and now it works. The only weird thing is that the UI of the app has been moved up and I don't know why either. (Picture attached) Since I don't have a ScrollBar, I unfortunately can't see half of the app. Maybe someone has an idea again? Best regards! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2021 09:49:48New subject after splitting |
|
Follow us on