9/15/2020 9:43 PM | |
Joined: 8/8/2017 Last visit: 7/3/2023 Posts: 5 Rating: (0) |
Im trying to install TIA v15 (Step7+WinCC Adv) on Windows 10 v1909. I was able to install and update v13 and v14 so far but just cant seem to get v15 installed. It will start the install, then about 2-3 minutes in it will say that there is ~20-25 minutes remaining but then say that the computer needs to be restarted to continue and that the install will resume after the restart. I confirmed that it created a scheduled task to start the install after the reboot but it never actually restarts. I then ran the task manually and it will start the install but it does the same thing over and over. Runs for a few minutes then says it needs to restart. I read through the logs but I cant really seem to identify where the issue is. Looking at the Summary log is seems the steps are all 'OK' and the last 'OK' is ClassicCompAfterUninstall. The it goes to "OKCallCurrentAfterReboot" for SetupUnit INSTSQL2014EXP. Seems like it might be having issues either installing SQL 2014 Express or Configuring it. Anyone know if these steps can be done manually? Attached some logs. Anyone able to assist? AttachmentSIA_STEP_7_PRO_WINCC_ADV_V15@20-09-15_12-18-02_summary.zip (56 Downloads) |
Follow us on