1/31/2018 7:33 AM | |
Joined: 4/28/2015 Last visit: 8/14/2023 Posts: 8 Rating: (0) |
Dear Expert I want to upload the parameters of the SINAMICS drive on the Profibus PLC network via Ethernet using the STARTER (v4.5) software. The CPU used is 412-2 DP (v5.3) and CP is used type 443-1 (v2.1) which supports routing. The inverter unit is SINAMICS G120 with CU240E-2DP firmware control unit (v4.4) I am using SIMATIC S7 (v5.5 + SP2) software installation on a computer with Windows professional 7. I have followed some of the instructions contained in this forum, but I still can not access SINAMICS drives via Ethernet. Note: to upload drive MICROMASTER 440 (v2.1 and v2.1) I have tried and succeeded, Please help me for the problem I am facing, for the supporting picture is in the attachment. Thank you very much
AttachmentSCREEN SHOOT.zip (185 Downloads) |
1/31/2018 8:41 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on