9/17/2021 8:24 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, APL uses signals as a structure. A boolean for example is created as struct consisting of a bool and byte. The byte is indicated as signal status and determines the status of the signal. A signal can have several statuses like simulated signal, bypassed signal, bad signal. The red wrench means that one of the inputs on the block (MotL) has a bad signal, so you must check the inputs and make sure the signal status is set to 16#80 which means the signal status is OK. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on