5/2/2007 10:46 AM | |
Posts: 19 Rating: (1) |
Hi, All the actions (are the file with .pas extention, not *.ftc or others)was located on the Server which contains only one picture named "start.pdl", not on Client. The picture I attached is a picture of the Client's. As you can see, the measurement value part is a customized object and was linked directly to internal tag from the Server. I have to take the conversion because I need to display and archivethe data after calculating from the SC. So the script of the actions have a following form: SetTagFloat("internal_tag",GetTagFloat("extenal_tag)*constant1/constant2); with the Upon Change update type of external_tag. AttachmentF01_Detail.zip (212 Downloads) |
Follow us on