2/11/2010 5:30 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
Hello, I have created a custom block in SCL and compiled and is then used in CFC. I have modified some VAR names and added a few. I compiled everything, but now I have to update this in the chart in CFC editor. When I drag the new compiled block in CFC, PCS7 prompt me that it is a new version. The block is then inserted. Because I have about 13 inputs and 13 outputs, I want to replace my existing block with the new block. otherwise I have to connect all my inputs and outputs again. Is there a way to do this? Thank you. |
If I could help you, you can use the RATE button. Thank you. |
|
2/12/2010 3:50 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
That is the solution! Thank you |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on