Industry Online Support
Technical Forum
3/2/2010 6:25 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi CoolCat, I found this FAQ http://support.automation.siemens.com/WW/view/en/21808321with this note: Note: The value in the memory area is only read at the next updating cycle of the tag addressed. If, for example, you use a multiplex tag in a script, after changing the memory area you do not directly access its content. => In a script, avoid changing the index of multiplex tags and then accessing those tags. Changing the index of multiplex tags and then accessing those tags (e.g. within the same script) can cause data inconsistency! |
mfG / Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on