4/13/2018 7:26 AM | |
Joined: 7/13/2007 Last visit: 2/9/2024 Posts: 32 Rating: (1) |
Hi, I am using IPC machine with Windows XP as a WinCC client in one of the projects. Now I am going to upgrade the OS to Windows 7 ENT (32 bit). We have following installed network adapters card in client machine: 1. Realtek RTL8168C(P)/8111C(P) PCI-E Gigabit Ethernet NIC 2. Siemens CP 1612 My query is: Will I have to upgraded the network adapters drivers after upgrading the OS from Windows XP to Windows 7 ENT.. If yes, from where I can download the drivers of these network adapter cards, suitable for Windows 7 ENT (32 bit) Screen shot of IPC's Device manager is attached for reference. Thanks! AttachmentNetwork Adapter_IPC.docx (271 Downloads) |
Follow us on