12/9/2020 2:43 PM | |
Joined: 12/8/2020 Last visit: 12/28/2020 Posts: 1 Rating:
|
Can anyone in Forum advise me to upload complete program from a Locked 1500 CPU, Customer lost Backup , CPU also locked. Is it possible to upload . It is Urgent please,
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/10/2020 11:03:46New subject after splitting |
|
12/9/2020 4:08 PM | |
Joined: 7/7/2010 Last visit: 3/4/2021 Posts: 10211 Rating:
|
To upload a locked PLC, do you mean the PLC has a password and nobody knows the password? You can use the SIMATIC Automation Tool to capture a complete backup of the running project. The tool can load the captured backup to a replacement should the current PLC fail. If you want the original logic / hardware configuration, you need the password used to lock the PLC project. This concept borders on the unethical - depending on perspective and application, but perhaps someone can use something like AutoIt! to brute force password attempts to unlock the PLC once you have a full backup loaded to a spare PLC.
|
science guy |
|
Follow us on