11/29/2015 11:16 AM | |
Joined: 9/16/2013 Last visit: 11/12/2023 Posts: 145 Rating: (16) |
Hello Error6662, first welcome to the forum. check that the configuration and the actual hardware configuration match. and perhaps the below link help you. https://support.industry.siemens.com/tf/ww/en/posts/station-upload-problem/34545/?page=0&pageSize=10 Regards hag010 |
Last edited by: hag010 at: 11/29/2015 11:17:35 AM |
|
This contribution was helpful to1 thankful Users |
11/30/2015 2:33 PM | |
Posts: 3 Rating: (0) |
than you for helping me according to your link , i try with Step7->Display acessible nodes i can see the blocks but none of them wont open ! :S |
7/31/2021 12:21 AM | |
Posts: 1 Rating: (0) |
hello CPU 414-3 type thıs smatıc manager v5.6 PLC IP adres 192.0.0.2 PC IP :192.0.0.100 SET PG/PC GbE famıly con. TCPIP.1 or TCPIP Auto fault code:33:16662 |
8/2/2021 3:26 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi sersan25, same subnetmask? how are the devices connected? by searching for the error-code on the upper rigth, you can find this: What is the meaning of the error codes (xxxx:yyyy) in STEP 7?due to the document in the FAQ 33:16662 has following cause: The partner is neither a CPU nor a CP. Are you sure that you have the rigth IP-address? regards, |
FCK WAR! |
|
Follow us on