3/22/2017 6:19 PM | |
Posts: 1 Rating: (0) |
Dear Expert. I need some help to Upload THE software from old siemens HMI. I am using ProSave to Upload. The Siemens Cables that I got with me are : PC Adaptar USB A2 ( 6GK1 571-0B00-0AA0 MPI/DP (6ES7972-0CA23-0XA0 The HMIs that I need to upload are : TP177B TP177A MP277 My questions are : 1 )Can I use PC Adaptar USB A2 ( 6GK1 571-0B00-0AA0 to upload from TP177A and TP177B ? or MPI/DP (6ES7972-0CA23-0XA0 ? 2 ) Do I need to change the DIP Switch on the back of the HMI (TP177A) to Upload ? 3) For MP277 what kind of cable do I need, can I use PC Adaptar USB A2 ( 6GK1 571-0B00-0AA0 to upload , or I Need RS232/PPI Cable 4) Do I need to select transfere Mode on the HMI to Upload by Prosave ? Thanks a lot ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/23/2017 9:56:15 AMNew subject after splitting |
|
3/22/2017 8:38 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, have you already seen this: http://support.automation.siemens.com/WW/view/en/19109408 and and |
Last edited by: Ste39 at: 3/22/2017 8:59:32 PM |
|
1/23/2018 9:43 AM | |
Posts: 4 Rating: (0) |
Hello, Is there any option to upload from TP177A and download it in TP177B. If there is any step by step procedure for this, Please share the same. |
1/23/2018 9:52 AM | |
Posts: 4 Rating: (0) |
I dont have the original project. Is there a way to upload the wincc flexible project from the HMI? |
2/22/2021 9:21 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147)
|
Hello, Do you have original project? Best regards, Wizard |
2/22/2021 9:28 AM | |
Joined: 4/3/2017 Last visit: 6/1/2023 Posts: 6 Rating: (0) |
Yes.I have the original project.. |
Follow us on