5/1/2014 8:04 AM | |
Posts: 13 Rating: (0) |
Dear Mr, Essence of the problem: When uploading the program from the controller S7-200 6ES7214 ... program TIA V11 (with connections other versions message appears - "project was created in a different version"), according to instructions - «How to Upload a Program and Configuration from a 1200 PLC» (attaching) performs Item 8 - «Compare offline / online». At this point lost connectivity with the controller (attaching the photo). Command "ping" performed well. Download the program impossible. What could be the problem? AttachmentC:\4\Compare.zip (181 Downloads) |
5/1/2014 3:24 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
If you are attempting to upload a project written in V10.5 of the portal, you may be out of luck with any version of the portal. If you are wanting to upload a project - presumably because it is not backed up anywhere - and have V11, if the project was written in V12 or V13, you will not be able to do it. If you have V11 and do not have SP2 and Update 5 installed, install SP2, then update 5, and any hardware support packs required to support the hardware in the project. Try again. If you have the latest V11 and you know the project is V11, then try this: Support Request If you want to keep using the portal software, you may want to upgrade to V13 (skip right over V12). V13 can work with V11, V12, and V13 projects. |
science guy |
|
6/12/2017 1:37 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by 23183356 is split to a separate thread with the subject TIA V11, can't upload to PG. Best regards |
Follow us on