9/4/2018 8:26 PM | |
Joined: 2/3/2011 Last visit: 5/8/2024 Posts: 345 Rating: (10) |
Hi, recently I upload a program from an 315-2 DP (6ES7315-2AF02-0AB0) but when I check consistency it shows some errors from simovert and micromaster drives configuration. What can I do to solve the error. I attached images from the hardware configuration and the errors. I´m using step 7 v5.5. I need this cause I want to replace the CPU with a new one (6ES7315-2AH14-0AB0) Thanks in advanced. AttachmentError.zip (156 Downloads) |
9/11/2018 10:46 PM | |
Joined: 2/3/2011 Last visit: 5/8/2024 Posts: 345 Rating: (10) |
Until yesterday I could test it, and it worked. In HW Config I errased all drives from the profibus network, before this you should check the I/O Addresses. If you don´t know the addresses you could view them by clicking View>Address Overview… It shows the address and the length of PKW and PZD. I just add the Masterdrive CBP , from the catalog, to the nertwork and configured the I/O Addresses. Used Step 7 5.5, also installed in PC DriveES SIMATIC 5.4 Hope this helps. AttachmentConfiguration.zip (141 Downloads) |
Last edited by: syd_b at: 9/11/2018 11:00:11 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on