5/5/2021 6:56 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello rachid; First step: the C7-635 manual: https://adegis.com/media/asset/29a6705fc30085c7f30dce5dedc18450e24f428ec30375df317a46c77a4b411e.pdf "The C7-635 consists of the following individual components: • SIMATIC S7-CPU 314C-2 DP • SIMATIC Touch Panel TP170 B (C7-635 Touch) and Operator Panel OP170 B (C7-635 Key)". Both components run independantly with different softwares. The PLC side requires Step 7 v5.6 (as you work with Windows 10). Chapter 19 of the Programming with Step 7 manual describes downloading and upploading procedures for S7-300 and S7-400 PLCs(look at the screenshot below). https://support.industry.siemens.com/cs/ww/en/view/109751825 Before you can upload from the C7, you must have a correct connection adapter or processor. + cable for MPI. A CP 5711 is often recommended: 6GK1571-1AA00, USB to MPI/Profibus adapter. You must also use a piece of software called the PG/PC Interface (inside Step 7) to enable the MPI driver for the adapter or processor, and to diagnose the connection. Don't hesitate to come back to us for more details, if required. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on