7/16/2013 3:27 PM | |
Posts: 49 Rating: (0) |
Hi When i upload S7-318-2DP, it is uploading but canot upload the comments. Is it possible to upload comment and HOW? Regards nadeem |
7/16/2013 3:33 PM | |
Posts: 49 Rating: (0) |
Hi-Suresh Can u explain more how it will byT1A? regards Nadeem |
7/16/2013 6:07 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, I don't think that you will get comments for S7300 CPUs even with TIA. I may be wrong. But Here is the FAQ for S71200 CPU with Screenshot so you can try in similar way for your CPU in case you are working with TIA in this case. In STEP 7 (TIA Portal) V11, how can you upload blocks from the CPU to the PG, for example, into a newly created project? hope this helps. |
VANDE MATARAM..... |
|
7/17/2013 7:12 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
In case of using Step7 5.x It's possible to save other files on the MMC: http://support.automation.siemens.com/WW/view/en/15399111 And the complete programm, including Symbols and Comments: http://support.automation.siemens.com/WW/view/en/14053219 |
This contribution was helpful to1 thankful Users |
7/19/2013 1:02 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Follow-up-question splitted to migrate my PLC programming from Step 7 to TIA portal Best regards O_Moderator |
Follow us on