5/24/2011 9:55 PM | |
Joined: 1/5/2007 Last visit: 11/30/2016 Posts: 1654 Rating:
|
Hello LOGO!-user, today I would like to present once a special feature near the block "comparator" that can be been useful absolutely for value displays in text messages to you. I tested this in the simulation and at real LOGO!-Modulen with display of the series 0BA5 and 0BA6. Usually the range of values of the analogous blocks is restricted on -32768 to 32767. If this limitation becomes a value effective then in particular by reference into a parameter of an analogous block to the program run time one "gets", and at every analogous block exit the value isy restricted. Even if one is indicated an actual value of an analogous block in a text message the display value correspondingly restricted. HOWEVER as a single block (as far as I explored this) the comparator behaves differently, because it is possible in a text message (and only there), actual values "Ax - Ay" (and only this!) to get the display in the value range of - 65354 to 65354 !!??!! .....Look for this purpose once the circuit<A[circuit|switching]> examples at the attachment ....I am tightened onto your comments on that. Best regards AttachmentDEMO_Komparator_Besonderheit.zip (84 Downloads) |
Last edited by: Betel at: 9/5/2013 9:52 PMCorrection: LOGO!-Soft version 7.1.5 solved this bug of the block comparator - now the PC-simulation is ok! ==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to
2 thankful Users |
4/23/2012 6:09 PM | |
Joined: 1/5/2007 Last visit: 11/30/2016 Posts: 1654 Rating:
|
Hello, are this information helpfull to you to program the LOGO!? Have youexamples for me or your own results of you experimental?. Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
5/30/2012 9:06 PM | |
Joined: 1/5/2007 Last visit: 11/30/2016 Posts: 1654 Rating:
|
Hello, the special effect of the block "comparator"cannot only used at textboxes! It is also possible to use the big value at the range of -65536 to 65535 in TIME-function blocks (as pointer) !!! Please look at the files at the attachment to learn about this possibilities.... Best regards Betel AttachmentDEMO_Komparator_Besonderheit_V2.zip (24 Downloads) |
==> Meine TAG-Listen: "deut." |
|
Follow us on