Industry Online Support
Technical Forum
11/12/2012 3:25 PM | |
Posts: 376 Rating: (57)
|
Hello nevio, I think that should work. Please checks whether your Siemens PC Adapter USB works with USB 2.0. The following information still would be interesting: 1. What kind of Windows Operating system do you use? 2. Which STEP 7 software has you installed? Version? 3. Which order number does your PC Adapter USB have? 4. Have you installed any software (driver) for the PC Adapter USB? Perhaps the information from this web side helps you. Make a click. http://pcsupport.about.com/od/findbyerrormessage/a/code-10-error.htm Good luck! If you have a solution for there problem, please inform us. Many people in this world are interested. Thank you very much. Best regards Azteke0110 |
11/13/2012 1:28 AM | |
Posts: 5 Rating: (0) |
Windows 7 32bit Step 7 5.5 PC Adapter 6ES7 972-0CB20-0XA0 Step 7 inbox drivers v8.1 or PC Adapter CD v2.0 driver for the PC Adapter USB |
Last edited by: nevio at: 11/13/2012 1:29 AM |
|
11/13/2012 12:29 PM | |
Posts: 376 Rating: (57)
|
Hello nevio, thanks for your send information. Please take into account. In SIMATIC STEP 7 V5.5 and other SIMATIC software products released for Windows 7, the required driver for the SIMATIC PC Adapter USB are part of SIMATIC Device Drivers. A separate installation of the drivers as before via the CD supplied together with the PC Adapter USB is thus no longer necessary. Please follow the notes in the following FAQ: http://support.automation.siemens.com/WW/view/en/44914248 I hope you have not installed the drivers of this CD “PC Adapter CD v2.0 driver for the PC Adapter USB” yet. For Windows 7 you must use the drivers from the SIMATIC Device Drivers. The driver on the CD "PC Adapter USB 10/2007" is not released for Windows 7. Try the following. Install STEP 7 V5.5 again. If you use only STEP 7 V5.5 without Service Pack. You find the current Service Packs here. http://support.automation.siemens.com/WW/view/en/43346624 Best regards Azteke0110 |
11/14/2012 6:27 AM | |
Posts: 5 Rating: (0) |
I feel the need to install the adapter USB3.0 drive. I can not find the adapter's USB 3.0 driver, and I hope you will provide links or drive. |
11/19/2012 2:09 AM | |
Posts: 5 Rating: (0) |
Anybody know? |
12/18/2012 12:31 PM | |
Posts: 18 Rating: (0) |
hi dear you have solution from this usb problem |
12/19/2012 1:18 AM | |
Posts: 5 Rating: (0) |
|
2/13/2013 8:52 AM | |
Posts: 18 Rating: (0) |
Dear navio u.s.b 3.0 is communicate from update sp5 u tried... thank you., |
Follow us on