10/19/2010 1:13 PM | |
Posts: 5 Rating: (0) |
Hi . Running XP in virtual mode with Windows 7. Can't get coms between PG and CPU. Have loaded drivers. Any one have the same problem? Regards |
10/19/2010 1:59 PM | |
Posts: 5 Rating: (0) |
Hi Miami. Have activated in the virtual mode. Gone into hard ware in XP ,does see the usb but with a " yellow ! " mark. Mabe a driver or something? Regards |
10/19/2010 3:20 PM | |
Posts: 947 Rating: (45) |
for work under VM need CP5711 |
10/19/2010 6:10 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326)
|
Yes you need a driver (at least in the virtual machine) It is included in STEP 7 V5.5 and inSTEP 7 V5.x (exept V5.5) you need this driver. PS: In the PCT Package (Free download for IO-Link) is the same file "SIMATIC Device Drivers.msi" included as in STEP 7 V5.5. So I expect, when you install this, you will get the actual driver for your USB Adaptern (But I don't know!) |
Last edited by: miami at: 10/19/2010 6:14 PM |
|
11/29/2010 8:10 AM | |
Posts: 5 Rating: (0) |
Thanks for all the help.Looking good |
11/1/2011 3:09 PM | |
Posts: 1 Rating: (0) |
I also tried this and it works. Well done Miami |
Follow us on