12/16/2020 4:25 PM | |
Joined: 10/19/2020 Last visit: 1/20/2021 Posts: 18 Rating:
|
Hello, I have an Archer T2U Plus USB Wi-Fi adapter that I want to use to connect to the IOT2040 to the internet. I have looked into both this discussion and this discussion that talked about connecting to the IOT2040, but had no luck. I do not see an option for "Configure Network Interfaces" in the iot2000setup and I do not get an option for wlan0 even when the USB stick is plugged in. Does anyone have any idea how to connect an Archer T2U Plus to the IOT2040? Do I need to put the driver files in a certain area of the IOT2040? If so, how do I get those files on my computer to transfer over? Any help would be very appreciated. Thanks |
Follow us on