5/27/2020 3:07 PM | |
Joined: 9/23/2005 Last visit: 9/23/2024 Posts: 4709 Rating: (721) |
Whenever you describe here some issue, pls follow these rules.
In FC2 create TEMP var of type UDT. Copy FC2 IN to TEMP, then use TEMP as IN for FC1. |
Regards, |
|
This contribution was helpful to1 thankful Users |
5/27/2020 3:14 PM | |
Joined: 4/22/2018 Last visit: 7/29/2024 Posts: 57 Rating: (2) |
Nice Rules! Thanks, Temp could be as an input. but I have another problem! :))) How can I move a UDT to another one? The "Move" block does not work for UDT.
|
5/30/2020 9:04 AM | |
Joined: 4/22/2018 Last visit: 7/29/2024 Posts: 57 Rating: (2) |
- Operating System: Windows 7 Ultimate - Tia Version: V15.1 - The Problem: Cannot Move a UDT which is a FC input in the FC. The input UDT cannot be used in the MOVE or BLKMOV block's input (Attached). Same error with function input in a function. The FC inputs are here.
AttachmentScreenshots.zip (77 Downloads) |
Last edited by: Jen_Moderator at: 06/02/2020 08:28:56Removed link and added all files as an zip file. |
|
Follow us on