5/20/2011 2:37 PM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308) |
Hello Ansigiangho,
Yes you can use the AO as long as the input impedance of the indicator is suitable for the AO module. Best regards. H-H |
5/21/2011 4:11 AM | |
Posts: 7 Rating: (0) |
Thank you. Because of voltage drop Max 1.1V, I think input indicator impedance is about 275 Ohm. It is okie? Siemes AO card can power for that one?
|
5/23/2011 9:36 AM | |
Posts: 7 Rating: (0) |
Dear Experts I attach specification of indicator for you. I just want to make sure that Siemens's AO module can used for powering to that indicator. Thanks in advance.
AttachmentP&F 130039_eng.pdf (354 Downloads) |
5/24/2011 6:19 AM | |
Posts: 7 Rating: (0) |
Dear Friends. Any help. I need it so mucn Thank you. |
Follow us on