Industry Online Support
Technical Forum
1/25/2011 11:10 AM | |
Posts: 2 Rating: (0) |
Thanks for your reply, another question: will the EWS see the other nodes via the MBI card or it will see only the node (APACS Rack) where it connected to? BR, |
7/14/2011 4:04 AM | |
Joined: 5/23/2006 Last visit: 3/27/2023 Posts: 16 Rating: (4) |
The EWS will see all stations that have an mbus or mnet connection to the rack that it is attached to. |