Industry Online Support
Technical Forum
9/11/2012 2:47 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, I suggest you read S7-200 SIMATIC Text Display (TD) User Manual The programming is done in Microwin with the TD wizard and then downloaded to the CPU, all you have to do in the TD is set the right CPU adres and some other communication settings. The cable between TD and CPU is a special TD cable (power supplied by CPU) or you can use profibus cable with connectors (external powersupply) If you have specific questions after reading the manual, please come back and ask. Regards, Marcjan |
Last edited by: Marcjan at: 9/11/2012 3:27 PMLast edited by: Marcjan at: 9/11/2012 2:48 PMProblem solved? |
|
This contribution was helpful to1 thankful Users |