11/30/2018 12:46 PM | |
Joined: 4/24/2006 Last visit: 4/15/2024 Posts: 8610 Rating: (1146) |
Hello, Perhaps this link might help: What additions are included in the firmware changes of the S7-1200 controllers? A CPU S7-1200 v4 can be used as IO device. Best regards, Wizard |
Last edited by: Wizard at: 11/30/2018 12:56:08 PM |
|
This contribution was helpful to1 thankful Users |
11/30/2018 1:14 PM | |
Joined: 2/10/2012 Last visit: 3/28/2024 Posts: 314 Rating: (58) |
That's fast! Thanks, that is what I was looking for. So V3 can be io-controller (max 16) and only V4 io-device. |
Follow us on