6/28/2013 1:28 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
You did configure the users and groups in the: Local users and groups? that is, on the OS computer |
If I could help you, you can use the RATE button. Thank you. |
|
6/29/2013 10:08 PM | |
Posts: 62 Rating: (4) |
I am working on PCS7 V7.1 SP4 in a project which has 2 redundant servers and 8 clients. The server and clients are communicating and data is being shown on clients. There are 12 picture areas in the navigation area. I want those all 12 picture areas to be visible for all the users in all the 8 clients. But I dont want everyone to operate in all the 12 areas. For this select the pic selection with area buttonsorpic selection with area buttons and group display. With this operator can view thescreens but he cant control the faceplates. this u need to do in Client Station I want users from Client 1 and Client 2 operate/control only in area 1 and area 2. Remaining areas should not be controlled by them but should be monitored by them. For this Please Refer Attach file file Name: user administration-Area Spe How do I accomplish this? What settings should I do in User Administration? Where should I do it? Server or Client? All these Settings to be done in OS client Only For trial, I tried creating 2 users in server and gave them different rights User1: Area for authorization, Process Controlling, Higher Process controlling was given only for 2 areas User2: Area for authorization, Process Controlling and Higher Process Controlling was given for reamaining 10 areas When I logged in using the User 1, I was not able to control also in the assigned areas. Same with User 2 as well. And One more thing is Using simatic Loging is Best for this Kind of application.configuration of simatic logon manual is avb in Pcs7 Manuals CD(pcs7 multi media CD-2) Regards, Avinashkrishna Bhimavarapu Attachmentosproject.zip (127 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on