9/21/2015 2:17 PM | |
Joined: 3/14/2008 Last visit: 5/6/2024 Posts: 2066 Rating: (928) |
Hello all, PCS7 6.1 SP4 We have multiclients that read several server packages from different installations. In order not to get alarms from all area's, several users are setup the way they have only authorization for several area's. Normally if you click the first "balloon" under "Authorization for area", you get access to all area's. But this is not the case right now. Everything is good, except the users have no authorization to modify user archives anymore. Also, trends which are restricted to a certain authorization, also not work. The authorization is present, but the system refuges to modify user archives. When I put back the original configuration-> authorization for all area's...everything is OK. How is this possible? Is this a bug of the system? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on