Industry Online Support
Technical Forum
5/10/2012 1:07 PM | |
Posts: 495 Rating: (58) |
Hello users, I want offer you my user defined function (UDF) for controlling shutters. Description Inputs, Outputs and Parameters: “Q_UP” and “Q_DOWN” are the outputs for the direction of the shutter. “I_UP” and “I_DOWN” are the inputs for set or reset the outputs. “FB_UP” and “FB_DOWN” are the feedback inputs. They are needed for locking the reverse direction while one direction is set. The parameters “T_U” and “T_D” are the off delay for the outputs. Function: A positive edge on the inputs “I_UP” or “I_DOWN” sets the corresponding output for the time which isadjusted in “T_U” or “T_D”. A second positive edge resets the output. A high signal at the inputs forlonger than 0,5 seconds sets the output as long as the high signal is there. Please give me feedback to the function! Regards Andreas AttachmentShutter.zip (467 Downloads) |
Last edited by: Mc Muffin at: 5/10/2012 1:07 PM |
|
This contribution was helpful to5 thankful Users |
Follow us on