5/21/2020 2:36 PM | |
Joined: 7/29/2013 Last visit: 4/19/2024 Posts: 52 Rating: (1) |
Hi, I´m facing a similar issue. But i´m working whit a IO Link master whit Profinet interface. The AL1102 from IFM. Looking over the manual (pag 37) says that the cap is 0xB400, that means hex B400? I´m using 16#B400 for CAP on FB50001 trying to read CGA parameter (Index 3008) of a flow sensor SA5000, but nothing happen. Can you help me please? https://www.ifm.com/mounting/80280033UK.pdf ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/25/2020 07:37:42New subject after splitting |
|
5/21/2020 4:22 PM | |
Joined: 7/29/2013 Last visit: 4/19/2024 Posts: 52 Rating: (1) |
Ok, Attached i´m posting two pictures. In the first one you can see the hardware config of AL1102 whit the HW ID 281 = 16#119 and the ports configuration as well. And other picture shows that i´m using FB50001 that i´m downloaded from Siemens support. There you can see the error code. For SA5000 flow sensor CGA parameter index = 3008 and sub index = 0. All this decimals not hex. The len is 32 bits and i´m not sure how should to expressed on FB if it need to be 4 bytes o 32 bits. The sensor is connected on port 5
AttachmentPictures.zip (193 Downloads) |
Follow us on