1/23/2019 10:22 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello zonouzi,
By testing in PCS 7 V7.1 you didn't use the Advanced Process Library but the PCS 7 Standard Library. So it seems that the "X" in the message related icons is specific from the APL. From PCS 7 V8.0 or higher PCS 7 Standard Library is no longer installed automatically via the frame setup. It is provided in the directory "Additional Products" on the PCS 7 DVD and can be installed manually. With the release of PCS 7 V8.1, the PCS 7 Standard Library is not available as version V8.1, but only as last released version V7.1.3.
And there is no small version for VlvMotL (FB1900) available. with regards |
Last edited by: Heisenberg2 at: 1/23/2019 3:07:56 PMLast edited by: Heisenberg2 at: 1/23/2019 3:08:30 PMLast edited by: Heisenberg2 at: 1/23/2019 3:13:08 PMLast edited by: Heisenberg2 at: 1/23/2019 3:14:32 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on