7/20/2016 12:52 PM | |
Posts: 18 Rating: (1) |
Hi Edek, Yes, block in FC and in Sources folder appears under different name. I do not see how to recognize that in CLI program. Dmitriy |
7/28/2016 12:34 PM | |
Joined: 7/20/2006 Last visit: 8/21/2024 Posts: 128 Rating: (8) |
Hi Here you will find some example. https://support.industry.siemens.com/tf/ww/en/posts/use-of-source-file/3716/?page=0&pageSize=10 regards Lukasz |
This contribution was helpful to1 thankful Users |
8/30/2016 3:53 PM | |
Posts: 14 Rating: (1) |
Hello ! I checked my program with your example and it seems that I forget the "blk." in the call of my method ^^" but after that I developp it with the help of this reference https://support.industry.siemens.com/tf/ww/en/posts/use-of-source-file/3716?page=0&pageSize=300 which was very helpfull and now I can extract all my Source files since my Block files Thkx V.much ! It must be possible with the GenerateSource function but I don't have any Help to search for. If someone have a response ? ^^" maybe an expert Siemens... but every help is welcome Thanks ! H.N Edit : In fact I find myself the response ^^ to extract all the Sources files from all the Blocks files in a SINGLE .awl file, you just have to generate the source files not from the block but from the block container ! BlockContainer.GenerateSource -> 1 awl file for all the sources files from all the block files Block.GenerateSource -> 1 awl for 1 source file from one block file |
Last edited by: hydrenoire at: 8/31/2016 1:13:34 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on