4/3/2012 1:47 PM | |
Joined: 11/15/2006 Last visit: 1/20/2021 Posts: 1319 Rating:
|
Do you have STEP7 V11 only or do you also have WinCC? |
Have Fun! |
|
4/4/2012 8:37 AM | |
Posts: 36 Rating:
|
i have only TIA PORTAL V11 SP2, no WINCC |
4/4/2012 12:45 PM | |
Joined: 8/31/2010 Last visit: 2/12/2021 Posts: 1496 Rating:
|
Hello MINKU, WinCC Flexible is a software product from Classic world. Whereas WinCC Advanced v11 is a software product in the TIA Portal world. So two of them are independent softwares. Then WinCC Advanced v11 is used to do the engineering of your HMI (panel) on a PC. But the engineering is done for the WinCC RT Advanced v11. Thisprinciple is same for WinCC Flexible also. (There it will be WinCC Flexible Advanced 2008 [ES] and WinCC Flexible 2008 Runtime [RT]). Hope it's clear now. SIMATIC NET OPC Server for S7-1200 - Release of SIMATIC NET OPC Servers Version 7.1 (Edition 2008 SP2) with S7-1200 Steps: How can you establish a connection between an S7-1200 PLC and SIMATIC NET OPC? Delivery Release for SIMATIC NET DVD V8.1(compatible with MS Windows 7 but not in Windows XP Still SIMATIC NET v7.1 + SP4 (SIMATIC NET PC Software, Edition 2008 + SP4) is compatible MS Windows XP. |
Like it? Rate it! |
|
Follow us on