10/28/2008 2:48 PM | |
Posts: 4 Rating: (0) |
I am using "Simotion D425, SMC20 and external absolute encoder" in my application. I want to read angle values from external absolute encoder. I configured Simotion D425, SMC20 and external absolute encoder in my program. and when I download this program I have a fault message "F07552(A) Drive encoder: Encoder configuration not supported.". Can you help me about this subject? Thanks. In the attachment: Application program AttachmentD425absu.zip (585 Downloads) |
Last edited by: yavuncu at: 10/28/2008 3:12 PMLast edited by: yavuncu at: 10/28/2008 3:10 PMLast edited by: yavuncu at: 10/28/2008 3:01 PM |
|
10/29/2008 4:04 PM | |
Posts: 4 Rating: (0) |
Can i read value from simotion D410 via X23 without SMC20? I will use the same absolute encoder. Encoder features: BaumerIVO, made in Germany GCA2W.A12A101 464130 3 04.08 10-30 VDC 5%RW 1024 Bin. SSI Thanks Attachmentabsolute_encoder.pdf (603 Downloads) |
Last edited by: yavuncu at: 10/29/2008 4:24 PM |
|
10/30/2008 6:15 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014)
|
Hello, yes the X23 connector on D410 supports this encoder. Regards Christoph |
10/30/2008 12:47 PM | |
Posts: 4 Rating: (0) |
Hello ChristophD |