Industry Online Support
Technical Forum
2/19/2014 8:42 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi colleagues, I need to know if it is possible to use with all its functions the new modules SM336 6F-AI HART for the ET 200M and the modules: digital module 8 F-DI Ex NAMUR, digital module 4 F-DO Ex 17.4V/40mA, analog HART module 4 F-AI Ex HART for the ET 200 iSP with the PCS7 v6.1 SP4. Here I see a solution for the PCS7 v6.1 SP2 but they don't specify if it is suitable for the SP4 : http://support.automation.siemens.com/WW/llisapi.dll/31481983?func=ll&objId=31481983&objAction=csView&nodeid0=12265765&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=content&subtype=133100 Thanks in advanced |
2/21/2014 3:55 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi Ralfinio, Thank you to respond, the catalog of the HW Config in the PCS7 v6.1 SP4 doesn't contain these modules by default. I already found a solution, I installed the softwares: S7 F-FH Systems V6.1 and the S7 F Configuration Pack V5.5 Service pack 8, both are compatible with the PCS7 v6.1 SP4 , following the instructions that appear here: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=28930789&caller=view <----- To see page 15 and https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=28570675&objAction=csOpen&nodeid0=12265765&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW and following the instructions from the document "PCS7_V6_compatibility_list(2013)" that says for the S7 F Systems : *19)With installation of the S7 F ConfigurationPack V5.5 SP4 or later, you will have to repeat the installation of the PCS 7 Library V6.x, V7.0.x or V7.1 to receive consistent data for the driver generator. AttachmentPCS7_V6_compatibility_list(2013).pdf (40 Downloads) |
Follow us on