Industry Online Support
Technical Forum
6/4/2010 2:09 PM | |
Posts: 5 Rating: (0) |
Hello everyone, first of all i have to say, this forum very useful to siemens hmi user, My problem is WinCC fleixible 2007 advanced sp1 is runing in my pc and i want to use tp 177B 4" , however this device there is not in device type list in WinCC fleixible 2007 i checked Hardware Support Packages (HSP) for WinCC flexible (https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=19241467&caller=view) but i didn't find tp 177B 4" can i use Flexible 2007 adv with this device, if i can't , i have winCC flexible 2008 compact edition ,is there any way to useWinCC fleixible 2007 advanced andwinCC flexible 2008 compact edition together thaks a lot i
|
6/4/2010 2:25 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, To use different version of WInCC Flex on the same OS isn't possible. look at What connections are there between the version designations in WinCC flexible? best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 6/4/2010 2:29 PMLast edited by: UMENCHO at: 6/4/2010 2:29 PM |
|
6/4/2010 2:39 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168)
|
Dear sinancak, Here is link: sales/delivery release: SIMATIC HMI TP 177B 4" color PN/DP You need at least WinCC flexible 2008 compact. And as UMENCHO already said, it is not possible to install two different versions of WinCC flexible on one Operating System. Best regards, Wizard |
6/4/2010 2:53 PM | |
Posts: 63 Rating: (39) |
Dear Sinancak It is not possible to run both software on a single OS PLEASE understand From Mayank Patel |