Industry Online Support
Technical Forum
6/13/2009 9:57 AM | |
Posts: 16 Rating: (0) |
Dear All, If any one has tried uss communication between s7200 and 6ra70 drive. I have tried standard program attached here. But could not do it. I want to have a back up of drive and plc. AttachmentUss200_e.pdf (215 Downloads) |
6/13/2009 10:15 AM | |
Posts: 76 Rating: (8) |
Hi, Please expalain the Errors you haveon USS_CTRL output. Good Luck! |
6/13/2009 10:20 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Raj007, Can you explain a litle bit more what you already done and what king of errors did you received? Also this issue has already discuss here. Look at S7-200 with Simoreg DC Master using USS protocol It can helps! About backups - in Simoreg 6ra70 you should to use drivemon The necessary cable pins descriptions you can find here in forum or in manual "Simoreg dc master compendium" How to connect with the drive you can find also in this manual. Then just go to "drive navigator" button and then select "Save drive parameter to file". About S7-200 - in Microwin when you connect with CPU, go to upload button and there you can select what exactly want to upload.(Program block, Data block, system block, ). Hope this will helps. Best regards Hristo Mihalev |
Last edited by: UMENCHO at: 6/13/2009 10:22 AM |
|