7/11/2013 7:36 AM | |
Joined: 3/15/2011 Last visit: 3/20/2024 Posts: 134 Rating: (9) |
have a look at foolwing thread.vector control - basicsHope this helps Ashutosh
|
7/11/2013 7:43 AM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
Vector Control is better. . |
7/11/2013 12:23 PM | |
Posts: 235 Rating: (52) |
where is it? |
7/11/2013 12:54 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello jeet; Here is the link to the posted thread: vector control - basics If you use the search box at the right of the page (with a search term such as "Vector control") you can find many more threads dealing with similar issues. Hope this helps, Daniel Chartier |
This contribution was helpful to3 thankful Users |
7/11/2013 1:03 PM | |
Posts: 9 Rating: (0) |
Hi all; You can also find valuable information from one of the Sinamics product Function Manual ex: G120 https://www.automation.siemens.com/doconweb/pdf/SINAMICS_1008_E/G120_FH.pdf?HTTPS=REDIR&p=1 after page 106lots of info about V/f &Vector Control Regards |
7/13/2013 11:43 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
In addition to above discussion, you can find nice detail in this Manual Vector control - should be used where high torque and precise speed control iss required where as V/F control can be used where not high torque at low speed is required Here is what MM440 OPI says The V/f characteristic represents the simplest control technique. In this case the stator voltage of the induction motor or synchronous motor is controlled proportionally to the stator frequency. This technique has proven itself for a wide range of "basic" applications, such as Pumps, fans Belt drives and similar processesWhen compared to V/f control, Vector control has the following advantages: Stable during load and setpoint changes Short rise times for setpoint changes (→ better control performance) Short rise times for load changes (→ better noise/disturbance characteristics) Accelerating and braking are possible with a max. adjustable torque The motor and driven machine are protected using the adjustable torque limit,both when motoring and regenerating The drive and braking torque are controlled independently of the speed Full holding torque is possible at 0 speed |
Last edited by: Vithani at: 7/13/2013 11:47 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
Follow us on