5/2/2018 6:02 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Refer this example. SINAMICS V: Speed Control of a V20 with S7-1200 (TIA portal) via USS® protocol/MODBUS RTU with HMI |
Last edited by: Jen_Moderator at: 5/2/2018 12:23:17 PMOptimized link. |
|
5/11/2018 6:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello andrewdaw1978, What I understood from your latest post is, you want to configure V20 without PLC but want to very speed by changing frequency from HMI. Is it correct? If yes, please refer SINAMICS V20 Inverter example where in you will find different predefined macro applications. You do not need external HMI since from BOP you can vary the set point/speed. If you want to use external HMI you will need PLC + HMI o set up communication with V20. HTH. |
Follow us on