6/28/2017 5:12 PM | |
Posts: 2 Rating: (0) |
Hi, we use the given node-red add-on from the first post and it seems to work, but sometimes we have the problem that the values of our Digital Inputs are "-1" and node-red crash. Any advice on how to resolve this error? Best wishes ------------------------------------------------------------------------------------------ |
Last edited by: ChrisPCherry at: 6/28/2017 5:13:37 PMLast edited by: Jen_Moderator at: 6/29/2017 2:07:05 PMNew subject after splitting |
|
6/29/2017 8:27 AM | |
Posts: 215 Rating: (6) |
Can you specify, when this behavior occurs? |
6/29/2017 9:27 AM | |
Posts: 215 Rating: (6) |
You have the pin M0 connected to 0V? |