5/31/2014 11:24 PM | |
Posts: 5225 Rating: (1185) |
oops.. The previous post was edited. Previously the output "FILTERED" did not receive a value. The ZIP file now has a "2" in the title. [sorry] |
6/1/2014 12:08 AM | |
Posts: 60 Rating: (0) |
Thank you Jens that was a real help. |
This contribution was helpful to2 thankful Users |
6/1/2014 9:36 AM | |
Posts: 72 Rating: (6) |
You can use the attached logic for signal filtering.Attachmentsmooth.zip (240 Downloads) |
6/1/2014 1:52 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
I guess this is matter of which version of STEP 7 Basic supports SCL.You should have "Generate Source files" from TIA V11 SP2 onwards for S7-1200 while I am sure that older should support that for S7-300/400. For filter, I sugget checking an SCL source file, developed by me, and it can be executed on S7-1200 (Just compiled).For sure , it also works in S7-300/400 as tested.
General notes on PLC programming AttachmentTIA_V11_SP2.zip (222 Downloads) |
Last edited by: hdhosseini at: 6/1/2014 1:58 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on