8/5/2006 11:05 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
[quote user="hamadi_insat"]I like to use the solution with RS 232. Hi H, With this solution you have to built a driverfor the VB-application, a CP340 RS232 canbe used to put the data to a PC RS232 port, further programming is on your own. Normally it is made by asking from the PC something with VB and then waiting for a answer. Easier is it to work withSIMATIC PRODAVE MPI V6.0where the routines are completly ready and you only have to use them. Then you don't need a CP340, you are using the MPI-portof the CPU. This is on base of RS485, you need then a PROFIBUS card in the PC, for example the CP5611. The routines are written in C# but can be used with VB [8)] Software Requirement: Operating system Windows 95/98/ME or Windows NT V4.x/2000/XP. Hardware Requirement: PRODAVE MPI V6.0 PRODAVE MPI V6.0 Mini Simatic PG or AT compatible industrial PC with 64MB main memory and MPI-ISA interface, CP5511, CP5611, CP 5512 or PC Adapter. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
11/13/2006 10:18 AM | |
Posts: 2 Rating: (0) |
We have developped a software wich can be communicate with S7-300 and S7-200. You can download an evaluation version of this here. |