10/18/2015 11:23 AM | |
Posts: 4 Rating: (0) |
I want to VBscript in Wincc V13. I don't know Where to Start. Can Pepple share me Document About VBScript WinCC V13. I sincerely thank. |
10/19/2015 4:26 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello phucuong231, here is a link to the VBS chapter in the manual of WinCC V13 SP1: Do you want your script to run on runtime Advanced or on a panel? There are differences if you want to access data on the panel/PC, because of the different operating systems. You can find more about that in the manual, if you need it. For beginning VBS I highly suggest the FAQ. In the manual you can find the syntax to each command. On the right side of the editor you can find often used function like if-then-else and you can use them easily. You can also select a system function, fill it out like you're used to, and afterwards import it into your script. Now you have the right syntax and don't have to worry about it. For more information search for VBS and filter for WinCC and FAQ or application example.
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to2 thankful Users |
10/24/2015 9:56 AM | |
Posts: 4 Rating: (0) |
thanks you |
Follow us on