Industry Online Support
Technical Forum
12/13/2013 10:41 PM | |
Posts: 16 Rating: (0) |
Typ tekst of een websiteadres of vertaal een document. How can I control the vbscript when the state of the tag is changed to 1 in tia portal v11. Thanks in advance.
|
12/14/2013 9:34 AM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Typ tekst of een websiteadres of vertaal een document. How can I control the vbscript when the state of the tag is changed to 1 in tia portal v11. Thanks in advance. Hello univers, You can configure a VBScript in a tag's 'change value' event. To do so, you open the HMI Tag table and thenclick ona tag and select the properties button of the inspector window. Now under events you should be able to find a event 'change value'. In which you can link the VBScripts. Hope this helps. |
Like it? Rate it! |
|
12/23/2013 9:21 PM | |
Posts: 16 Rating: (0) |
Oke thanks |
This contribution was helpful to1 thankful Users |
Follow us on